This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Use dual power supply, VS+=+2.5V,VS-=-2.5V,under this power supply condition, LMH6401 work normally. But if use single power supply,VS+=5V,VS-=0V,under this power supply condition, LMH6401 can't work well.The output just like PD pin been set to high,and i make sure it set been set to low, i didn't mount the jump on Jpd.
Hi Johnsen,
Just to clarify, the power down pin is being pulled low when you use a single supply? Is that correct? Also, what is the value of your VOCM pin when you use the part with a single 5V supply?
Regards,
Hi Jacob:
I just left Jpd disconnect. Because I find PD pin has a internal pull down resistor in datasheet. And I left Jpd disconnect when test on dual power condition.
When I use a single 5V supply, I didn't meansure the value of VOCM, and I didn't supply an extra power for VOCM.
Hi Johnsen,
How are you measuring the output of the amplifier? When you are using it on a single supply, the output's will be biased at 2.5V common mode by default. If you are using ground referenced test equipment, then that may be a problem.
Regards,