In the T I D A-0 1 0 0 1 9 schematic(page3) I see 10K resistors on both the inputs.Is this design choice just for current limiting on input pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the T I D A-0 1 0 0 1 9 schematic(page3) I see 10K resistors on both the inputs.Is this design choice just for current limiting on input pins?
Hi Jagbir,
Are you referring to R77 and R82?
-Tamara
Hi Jagbir,
they are not only for current limiting but also for low pass filtering in combination with C69, C70 and C73.
Kai
Thanks Kai !
What value is added to the design by R76 and R81. They could have easily been combined with R77 and R82.
Hi Jagbir,
R76 and R81 are necessary to limit the current through the protection diodes D12 and D13. R77 and R82 provide a further current limiting caused by the rest overvoltage dropping across the protection diodes. R77 and R82 also provide a low pass filtering, as these resistors are dominating over R76 and R81.
Kai