This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA820: High current output (46mA) rising edge slew rate

Part Number: OPA820
Other Parts Discussed in Thread: DEM-OPA-SOT-1A, , TINA-TI

Hallo,

I can not verify the Noninverting Pulse Response in our applikation.

VCC=6.2V...10V, VSS=-2V, Gain=+1, Pulse Signal High Level 4.6V, Pulse Signal Low Level 1V

Load: 50R series resistor+50R input resistance oscilloscop

Testboard TI DEM-OPA-SOT-1A

C1, M1, M2, M3: Output OPA820 for different VCC Values

C2: Input OPA820 (Generator)

Is the measured rising edge slew rate correct?

Regards