This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
By checking the LM318 specs, auxiliary circuits page 10, besides the offset adjust solution which is quite common, I see also the possibility to balance for increased slew rate. Because of some influencing, is it realistic/workable to combine these two solutions on one OpAmp? Thanks in advance.
Morning Willem,
I suppose you are talking about this figure.
1. The offset adjust is in the input stage - a DC balancing, but it does not improve drift
2. The slewing feedforward seems pretty crude, inverting only and probably injecting signal into the comp.node if the error voltage shows a transient to couple through -not going to improve settling time with that AC coupled path.
You can use both in one design, but why you would be looking at this when there are so many much better improved devices is a mystery.
Hi Michael,
Of course there are much, much better OpAmps, but I am focussing on types without using a electron microscope and which I can solder myself. And, the price is also taken into account. The LM318-N is a replacement type for the original LF357 which is obsolete. Q: If you have a better replacement, I'll buy you a beer :-) All in all, thank you so far.
Regards, Willem.
Yes, this X-ref works better. It seems that I have a different X-ref on the TI-site so far: BOM & Cross reference tool gives a different output. I you can provide the link I am happy, thanks!
Yes, this is an older internal one drawing on the SelGuide parametric database, the new one you are probably looking at is a 3rd party database,
http://www.ti.com/amplifier-circuit/op-amps/cross-reference.html
Michael, pretty ancient but the LM318 is still not a bad best choice; although pretty noisy, VCC max 40V, high GBW and slew rate. I'll go for it. Thanks for help.
Hello Willem,
LM318 is the lowest cost amplifier with that level of slew rate ability. uA733 is different beast but is similar in cost and speed.
Here is a search by slew rate for amplifiers that have a PDIP option.
http://www.ti.com/amplifier-circuit/op-amps/products.html#p2954=PDIP&sort=p22typ;desc
Hi Ron,
Thank you for your reaction, my question was solved already. I forgot to push the resolved button.
Rgds, Willem.