We are depending on an accurate solution to the INA117 scaling as described in TI sboa001 “Increasing INA117 Differential Input Range”. Essentially this is Vout = V3 – V2 + 19xV5 – 18xV1. The INA117A claims accuracy of better than 0.02%. In our initial development this was the case, and we were getting readings with <1% error. Our latest build has shown much greater error and we are coming to believe that the laser trimming does not include all of the internal resistors. We are looking for clarification on the specifications.