This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
could you please help to find documentation on TLV2372IGKR with information about marking on TOP and Back side of component, and also decoder of label on reel for same position?
Thank you in advance
Hello Oleg,
The only thing fixed is the "APG" text which is the part number code. Y=year, M=month, S =site, LLLL= is 4 digit lot code, [.] is an alignment dot
Top of package: top line = {TI logo} [Y][M], bottom line = [.]APG
Bottom of package: top line = [.] [Y][M][S], bottom line = [LLLL]
Can you provide a reel label example?
Oleg,
On top line, 8B fills in [Y][M] Y=8, M=B,
So year is 2018 with the last digit being set by the 8
So month is November with the month set by the B; Month is a simple hexadecimal conversion. So there will be no 0, nor letters D to Z
This has been fun, but I suspect there is a specific (yet, undiscussed) reason why we are discussing this. What is the issue that you are having with this reel of devices?
Oleg,
It looks legit to me. I like the '88' on the bottom as that is August 2018 which predates the reel sealing data of Oct 26, 2018. The previous supplied '8B' code did not make sense. The Z516 is a cryptic code as it should be. If you retake the label picture, I will ask if the package code matches the reel label.
Hello Ronald,
So, first line on top and bottom sides has the same meaning, and should be same or can be different as well? And what means H on bottom side?
Best Regards,
Oleg
Oleg,
Year =year and month = month, so that'll match. I'll paste in the first response as the answers are there.
The only thing fixed is the "APG" text which is the part number code. Y=year, M=month, S =site, LLLL= is 4 digit lot code, [.] is an alignment dot
Top of package: top line = {TI logo} [Y][M], bottom line = [.]APG
Bottom of package: top line = [.] [Y][M][S], bottom line = [LLLL]