This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ..
We are using TLV4170 as an instrumentation amplifier configuration with single supply voltage topology. What we are facing the issue is with 3.3Volts supply. For 5v supply , no issues were found. The issue was the amplification not happened when simulating through TINA software when we using 3.3 Volts. Can you please help in this issue. Attached was the schematic in TIna
Regards..
Sandeep. signamp_tlv.TSC
Sandeep, Welcome to the e2e forums.
The OPA4170 is not rail to rail input. The model will have poor results as a warning when the input range is close to the end. The OPA4170 can run on 3.3V, however it is not the best idea as the input range limitations will require careful attention. At 3.3V or even 5V, there are many better choices, such as TLV9004