Hi All,
I have a question regarding the power supply of the LMV339 comparator to be used on a new customer project.
The questions are:
• Is it good to power the LMV339 at + 5V?
• if so what margin do we have?
• why in the absolute maximum ratings Vcc max = 5.5V and in the recommended operating conditions Vcc max = 5.5V? Why do the two data coincide?
In summary, I would need a response for the correctness of powering the integrated at + 5V and understanding what the tolerances can be met on the value of the power supply.
Many Thanks,
Antonio