Part Number: OPA552
Other Parts Discussed in Thread: TINA-TI, OPA657, OPA846, OPA847, OPA837
We would like clarification on section 8.2.2.3 of the corresponding (OPA55x) data sheet. It is poorly written, and we can not decipher the "formulae" for determining the appropriate compensation capacitance values.
We need the formula to configure the compensation circuit to utilize the high slew rate of the OPA552 at gains between -1dB and -4dB.
We aren't even able to extrapolate the formula used to determine the capacitance values in the example (compensation for 1 dB gain) as it does not make much sense.
Determining the NG1 and NG2 values is made clear, but nothing else is clear.
How is it that the example NG1 value of "2", and the example NG2 value of "10" can possibly equate a -3dB pole frequency of 956 kHz using the GBP value of 12 MHz?