This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Olivier,
OPA333-Q1 is AEC-Q100 Qualified for automotive application, which the part has to comply to the following qualification difference. Also, only SOT-23 package in OPA333AQDBVRQ1 is qualified for the requirements.
It is very similar to parts that rated for Military and Aerospace application. Sometimes they have the same die with the same or slightly different IC packages. However, these parts are produced with more controlled fabrication process, which random selected parts will have go through the stringent qualification process for a given application, and meet the performance requirements, see the attached table below.
Best,
Raymond