Hello,
My customer would like to know the following parameters for OP07D.
Are these values available?
1.
TYP for Common mode input resistance
2.
MAX for equivalent input noise voltage
3.
Max for equivalent input noise current
4.
MAX and TYP for PSRR
5.
Power dissipation is defined as 80mW(TYP) and 150mW(MAX) for “Vo=0, No load” condition in the datasheet.
What is the voltage for these values, TYP and MAX?
Regards,
Oba