Other Parts Discussed in Thread: TLV3202
Hi team,
I have an issue in using TLV3202 as a comparator. While testing I supply Non inverting input (IN+) with frequency signal of 50% duty (Typically fat Low - 0V to High-3.3V levels) and Inverting input (IN-) with a reference voltage.
- Circuit works as intended when Input voltage High level is more than the Reference voltage. I.e. Output same frequency with 0-5V level.
- When reference voltage increased and made it more than input High level, the output supposed to be continuous 0V. But I get unintended pulse for ~100ns at each input pulse. This shall be observed from KHz to MHz range inputs and with almost 1.5V difference between input High and Reference voltage.
Circuit used for testing (Refer Only OUT1 comparator for below shown cases and waveforms)
Case 1 : Input(Non inverting) = 0 to 3.3V, 100kHz, 50% duty, Vref1(Inverting Input) = 2.5V to 3.2V. (Tested for different reference and same behavior observed)
Result : Out1 as expected. Waveform below
Case 2 : Input(Non inverting) = 0 to 3.3V, 100kHz, 50% duty, Vref1(Inverting Input) = 3.5V to 5V. Tested at different levels and output is same as attached waveform. What could be the cause of this unintended pulse and how to overcome this?