Part Number: OPA858
Hello,
I am trying to calculate the overall input capacitance of my transimpedance amplifier.
I am using the OPA858 with Ccm=0.62pF and Cdiff=0.2pF in single supply mode.
Since I am using a capacitive tee network in my feedback path, I was wondering if anyone knows if I am doing the calculation right.
The equivalent capacity of the tee network is calculated: Ceq = Cf1*Cf2/(Cf1+Cf2+Cf3)
Without the tee network (using only one feedback capacitor):
Cin = Ccm2 + Cdiff + Cj
Is it right that with the tee the input capacity is calculated:
Cin = Ccm2 + Cdiff + Cj + Cx
with Cx = Cf1*Cf3/(Cf1 + Cf3)
Thank you in advance,
Sonja