Part Number: OPA549
I am working with three OPA549T devices. Each is fed with a 10Vrms, 400Hz input and requires an output up to 5.00Arms at 10Vrms. Current is limited to 8A for each amplifier. The op-amps are supplied with +/-15VDC rails. There is a 247 CFM fan cooling the op-amps.
I think the performance issues I'm having come down to the incorrect heat sink size and poor thermal compound between the case and heat sink, but I want to make sure that I'm not missing something.
My worst case Power Dissipated, with the load a peak current of 1.6 Ohms, is (15V)^2/1.6 Ohms * 0.2 = 28.125W.
I am currently using RA-T2X-25E heat sinks from Ohmite. I think I need their RA-T2X-64E.
The thermal pad available was a poor choice, they are 175-6-220P pads from Wakefield-Vette. They don't cover the full case-to-sink interface and don't conduct heat as well as required; I think I need better than the 0.40 C/W thermal resistance of those pads.
Attached is an image of the behavior seen at the 5.00Arms load. I'm outputting about 4.00Arms with the imaged waveform.
Beyond the obvious issue with the thermal pad, are there considerations I'm missing to resolve this performance issue? Would there be a benefit to adjusting the supply voltages to the op-amp? Do you agree that a larger heat sink is required?