Hi Sirs,
According to the official specifications, the VIH(max) is 0.3*VDD with I2C and 0.8V with SMBus, while the INA231 defines VIL(max) at 0.4V, which is not in line with SMBus and I2C standards. Would you please advise if the INA231 can compatible with devices with 0.6V~0.7V VOL(max)?
SMBus Specification
INA231 Specification:
Thank you and Best regards,
Wayne Chen
06/02/2020