Hi Team,
The common mode input voltage range of LMV331 with 5V power supply is -0.1~4.2V. In 9.2.2.1 section, it's said that the input voltage range should keep lower than Vcc-0.7V and when IN- and IN+ are both higher than common mode, the output is low and output resistor is sinking current. In the maximum rating table, it shows the input voltage range should be within 0 to Vcc+. Does it mean the IN+ and IN- can be greater than the common mode voltage range without damage the device but if the input voltage is beyond 0~Vcc+, it may be damaged?