Other Parts Discussed in Thread: THS4541, LMH6554
Hello,
Customer use a full differential operation amplifier LMH6552. In practice, there is a error between out+ and out-. I use TINA to simulate the FDA LMH6552, with different differential input values (100mV, 500mV, 1000mV, 1500mV...) and 0V to VCM. For FDA, out+ and out- should no DC error. Through simulation, it can be found that there is a constant error (4.73mV) between out+ and out-. I want to know what is the cause of the error. Is it a problem of simulation model parameters? the FDA LMH6552 itself? or other?
The following are the simulation results.
When Vin=100mV, error=51.61-46.88=4.73mV
When Vin=500mV, error=251.33-246.6=4.73mV;
When Vin=1V, error=500.97-496.24=4.73mV
When Vin=1.5V, error=750.62-745.89=4.73mV