Hi team,
1. Here is the circuit which achieve the -18V DC to -12V DC via TL072 and the load is about 10mA. The input and V- is connected to -18V and VDD is connected to the GND.
2. could you help me double check the schematic to see if there is any improvement on the circuit.
Best Regards
Wesley Huang