This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309: PGA309 Multi-Cal Communication Error

Part Number: PGA309

I have been struggling with communication errors with the Multi-Cal system. 


Yesterday, i successfully calibrated a 4-20mA transmitter.  After calibration, I used the muli-cal system/program (Rev J) to read the EEPROM.  After reading the EEPROM on the 4-20mA unit, its output pinned at 2.22mA and was not responding to pressure stimulus (no change in output).  I power cycled the unit and still the output remained pinned.  I think stared a new calibration on the unit and was able to get the unit to function again.  However, if i read the EEPROM, the same issue would occur. 

Today, I tried calibrating a 0-5VDC unit.  The unit was already calibrated prior to installing it into the system.  When it was hooked up, the unit functioned and showed voltage output changing with pressure input.  I then tried to read the EEPROM for this unit.  It seemed to successfully read the EEPROM.  However, when i went to recalibrate the unit, i got a "communication error".  I then tried to re-read the EEPROM for this unit and I got erroneous data (all registers read 0A0A (hex). 

Is there an issue with the software that causes this issue?  What could be the problem?

Regards,

Avi

  • just tried using the Iout Pre-cal file for the voltage output unit and was able to successfully communicate.  This unit is definitely a voltage unit as it was giving a 0-5VDC output prior to these communication issues...

    Is something wrong with this hardware?

    Hoping someone can help soon!

  • Hello Avi,

    Most common questions and issues related to the PGA309 interface communication are frequently related to the PRG One-Wire interface settings. The PGA309 PRG interface register settings need to be set properly to support either 3-wire or 4-wire voltage output modules or current output modules.  Depending on the One-Wire interface settings, there may be a time interval restriction to establish communication to the PGA309 One-Wire interface. The Multi-Cal system only uses the PRG One-wire interface to communicate with the PGA309 or the EEPROM (the I2C 2-wire EEPROM interface is not directly accessible) 

    For example, on "three-wire" voltage output modules, the PRG is connected to the Vout pin, and the PGA309 PRG interface communication can only be accessed for a few milliseconds after power up, after this delay, the interface becomes inactive, and communication is no longer accessible and the amplifier Vout is active. Therefore, when using the device with OWD set to ‘1’ (Register 4, bit D15, One-wire Disable), the time interval after power-up is the only opportunity that an external communications controller can initiate digital communication with the PGA309 and trigger a one second delay in the internal state machine. After VOUT is enabled, no further digital communication is possible, unless power is cycled.

    I will attempt to reproduce the issue on the Multi-Cal system.

    Please provide the following information:

    1) Is the OWD (Register 4, bit D15, One-wire Disable) set to '1' on your application? 

    2) Please share the Pre-Cal file and/or model file of the 4-20mA Current Sensor.

    3) Please share the schematic of the Current-Output 4-20mA PGA309 test card showing the DSUB-9 connector to the muti-cal interface card connection.  If this is a PGA309 test card with selectable jumpers, please show the jumper positions on the PGA309 board test card.  If you are connecting the PGA309 sensor board to the Multi-Cal Interface board using the screw terminal block, please show a diagram of the terminal block sensor to Muti-Cal Interface connections.

    4) If the issue is also occurring on the voltage output sensor, please clarify if this is a 4-wire or 3-wire voltage output sensor.  Please share the Pre-Cal file and/or model file of this voltage output sensor.

    5) Please also share the schematic of the voltage-output PGA309 test card showing the connections to the PGA309 Multi-Cal interface board. If you are connecting using the screw terminal block, please show a diagram of the terminal block to Muti-Cal Interface connections.

    I will get a hold of the Multi-Cal system and set it up to attempt to reproduce the issue. 

    Please provide all the information above and allow a few days.

    Thank you and Regards,

    Luis 

     

  • Luis,

    Thanks so much for the thorough reply.  Here are the answers to your questions:

    1)  OWD is NOT enabled though when i pressed "read EEPROM" on the program, the check box that says "Iout+OWD?" was checked.

    2) I've attached the precal file for the 4-20mA unit. 

    3) My multi-cal system did not come with a PGA309 test card.  I've asked about this before and was told this wasn't available.  If it is, how can I get one? A test card would be VERY helpful in debugging these kind of issues. 

    4) I believe I've resolved the communication issue with the voltage board.   The jumper cable connected the common of the two power supplies seemed to be loose/faulty.  Once i replaced this, communication worked with no issue. 

    Iout.txt
    [PGA309_Settings]
    Numb Reg=3    
    Poly Order=2    
    Output Mode=2    
    Vout_High_Target=3.803221    
    Vout_Module_High_Target=0.000000    
    Vout_Module_Low_Target=0.000000    
    Iout_High_Target=0.020000    
    Iout_Low_Target=0.004000    
    Vout_Low_Target=0.395221    
    Vs=5.000000    
    Vref=4.096000    
    Calibrate Nonlin=TRUE    
    Calibrate Coarse Offset=TRUE    
    Reg0=0    
    Reg1=0    
    Reg2=0    
    Reg3=1280    
    Reg4=0    
    Reg5=0    
    Reg6=1027    
    Reg7=0    
    Reg8=0    
    Temp0=-35.000000    
    Temp1=25.000000    
    Temp2=80.000000    
    XTR_R1=11300.000000    
    XTR_R2=10000.000000    
    XTR_R_ref=191000.000000    
    XTR_Vref=4.096000    
    Secondary Output Stage=FALSE    
    Second Stage Gain=1.000000    
    Second Stage Offset=0.000000    

  • Hi Avi,

    By PGA309 test card, I was referring to the Custom PGA309 + sensor board schematic you are currently using.  Please provide your Custom sensor board PGA309 schematic showing the DSUB-9 connector to the Muti-Cal interface card connections.  If you are connecting using the screw terminal block, please show a diagram of the terminal block to Muti-Cal Interface connections.  If you don't wish to share the schematic publicly, you could start a private conversation

    Since TI already offers the PGA309EVM-USB for Customer evaluation, there is no PGA309 test card board offered on TI Store. However, if you wish, I could look into provide you a PGA309 test card Altium design files of a prototype if you are interested via private conversation.

    Thank you and Regards,

    Luis

  • Hi Patel,

    Thank you.

    I will review in detail and attempt to reproduce on the lab.  Please allow a couple of business days to access and setup the system.

    Kind Regards,

    Luis

  • This conversation is on-going via private conversation.

    Regards,

    Luis