This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3541: PSpice Model for TLV354x doesn't work

Part Number: TLV3541
Other Parts Discussed in Thread: TINA-TI

Hi,
I use TLV354x PSpice Model (Rev. A) SBOMA83A.ZIP (13 KB) - PSpice Model in Cadence Orcad 17.2.
If I simulate TLV354 Test Circuit.opj, it runs. If I change the power supply to non-symmetric voltages (for instance to +3.5 V / -1.5 V) and nothing else, it never runs. Not very useful for a Single Supply Op Amp.
I need a working PSpice-Model for Single Supply Operation - even better a PSpice-Model, which always works!
Regards!
Andree

Test Circuit Tran.out.1.zip