Hi,
Each product's top marking is applied as shown below.
TLV2371QDBVRQ1 : 317Q
TLV2371IDBVR : VBGI
What does each top marking mean?
If there is any material that you can refer to regarding top marking, please forward it.
Thanks.
Regards,
MJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Each product's top marking is applied as shown below.
TLV2371QDBVRQ1 : 317Q
TLV2371IDBVR : VBGI
What does each top marking mean?
If there is any material that you can refer to regarding top marking, please forward it.
Thanks.
Regards,
MJ
Hello MJ,
Parts are getting smaller so the full part number does not fit. The short code plus the package type and pin count reveal the full part number using this tool.
Hi, Ronald
I know what you said.
What I'm curious about is marking No. This is what 3, 7, 1, and Q mean in 371Q.
Can you tell us what each letter means?
If you have related materials, please provide them.
Thanks.
Regards,
MJ
Hi, Ronald
Thank you for your answer.
So, what does the VBGI marking of TLV2371IDBVR mean?
Thanks.
Regards,
MJ
MJ,
The individual characters have no meaning by themselves.
The full set does have a meaning that may or may not reflect the devices' part number
In this case it does not reflect. VBGI is a 5 pin SOT-23 means one of the following
TLV2371IDBVR
TLV2371IDBVRG4
TLV2371IDBVT
TLV2371IDBVTG4
No difference in four other than reel size.
Hi, Ronald
Thank you for your reply.
I will deliver questions from customers.
Please, reply.
Regarding the marking, it is expected that code related to the fab site, assembly site, and test site will be included. Isn't it?
It seems that the last character of VBGI or 371Q will be divided into industrial grade or automotive grade, which is the temperature range.
Thanks.
Regards,
Mj
MJ,
The last character matching is not always arbitrary; nor is it always certain.
It is always best to verify only using this tool or the data sheet.
For fab site, assembly site, and test site refer to the reel box labeling sticker.