Part Number: THS4631
Hello Support team,
I want to know more detail regarding below post.
THS4631 input bias current - Amplifiers forum - Amplifiers - TI E2E support forums
I've built a circuit similar to the one in the previous question.
I'm attaching a document in which I checked the operation.Inquiry_THS4631_input-bias-current.pdf
When the frequency of the AC voltage applied to the THS4631 was increased (1MHz),it was confirmed that a large DC offset voltage was generated.
Is the cause of this really an increase in the net current, the AC component?
Why does an increase in the net current of the AC component cause an increase in the DC offset voltage?
If net-current is an AC component, I imagine that net-current swings to the same magnitude on the positive and negative sides, centered at zero.
I suspect that increasing the net current (AC) does not increase the DC offset voltage when it flows into the outer impedance of the THS4631.
Best Regards,