This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2901-Q1: Common mode input_Simulation_Pspice

Part Number: LM2901-Q1
Other Parts Discussed in Thread: LM2901, LM339, LM393B
Hi,
During simulation of LM2901QPWRQ1 using LM2901.5_1 Pspice model in OrCad, following was observed.

Even if both the inputs at inverting and non-inverting terminals are out of common mode range, LM2901QPWRQ1 comparator is
working fine in simulation.
Vcc = 3.3V, Vcm =   3.3-1.5 = 1.8V
VRef = 2.5 at non inverting terminal via voltage divider from 3.3V.
Vin at inverting terminal, triangular pulse, 0 to 5V.
 
At output, I am getting nice pulsed output as if common mode range violation  doesn't have any adverse effect on ouput.
From Datasheet:
"When IN– and IN+ are both higher than common-mode, then the output is low and the output transistor is
sinking current."
Is it expected behavior of LM2901 in simulation?
Thanks in advance,
Sunney