Other Parts Discussed in Thread: THS3115, OPA2690, OPA690, OPA2889, OPA2890, OPA2625
Hi Team,
We would like to request your help regarding the customer's inquiry below.
I am looking op-amp similar to ths4032 but with enable bit. It doesnt need to be exact to ths4032, at least similar but with enable bit. Initially I look at THS3115 and I exited, however when I read further, this is current feedback and I need good DC accuracy for ADC testing. Here is my use case for the opamp
Supply : -3 to 9V
Type : Voltage Feedback for DC accuracy
BW : <50Mhz
MUST use shutdown/enable pins. This pin will be tied to voltage pin to control.
Noise : <6nV/sqrt
The opamp will be used as unity gain Single input SARADC.
Thank you for your support!
Regards,
Danilo