This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 1405
I posted this question in the Power Management forum without thinking. I believe this forum is more relevant.
I'm working on implementing current / voltage sensing for a (hopefully grid-connectable) 250W solar micro-inverter. Planning to use SM73308 for the PV panel DC measurements, but I am unsure what is the optimal component for measuring the AC output; I presume magnetic sensing would be better in terms of electrical isolation. I am in India, where mains power is 220V / 50 Hz.
Guidance is appreciated, as electrical hardware/power is not my main field.
Thanks,Anand Lobo
"Ignorance more often begets confidence than does knowledge." -- Bertrand Russell
Hello Anand,
There are two parts I would recommend for isolated current measurement on the AC side of the inverter: AMC1200 (http://www.ti.com/product/amc1200) and DRV401 (http://www.ti.com/product/drv401)
The AMC1200 is an isolation amplifier that interfaces to a shunt resistor, the DRV401 interfaces to closed loop-magnetic current sensors.
Best,
Jose Duenas
In reply to Jose Duenas:
Hi Jose,
Thank you, I believe I will go with the AMC1200 for simplicity.
Based on the solar micro-inverter block diagram (http://www.ti.com/solution/solar-micro-inverter-diagram), could you advise me if the components I've chosen (marked in the attached image) will be an effective solution? The solar panel I'll be using is this: www.moserbaersolar.com/resources/MBVP-CAAP-BB-english.pdf (245 Wp)
In reply to Anand Lobo:
Your selections seem appropriate. One component that you will need as well is a microcontroller to run the PLC communication protocol. In our TMDSPLCKIT-V3 (http://www.ti.com/tool/tmdsplckit-v3) we use the TMS320F28069.
Best regards,
Jose