Hi all,
I have simulated below circuit to get the measurements from a sensor. Sensor changes it's voltage 0-5V range. I wanted to convert it to a fully differential signal( -5 to 5V) to transmit to another circuit board. Then converted it in to a single ended signal and scaled it down to 0-3.3V measurement to get reading to micro-controller. My simulation is as below and simulation results were as I was expected,
But after implementing circuit with 1% resistors, I couldn't even get close results as I was expected in simulations. I think I have made a mistake with choosing LM318 and seems it may not suit for this application. Now I want to change the LM318 from the circuit and test it back to get close results as simulations.
Voltage following (buffering) stage added some offset to the signal. My supply voltage is+15V/-15V.
1) How can I chose op-amp for voltage following stage and the scaling stage ? what are your recommendations?
2) What are the main differences between OPA,TLV,TLE,LM op-amp series?
3) Further I have voltage adding and subtracting circuits as well. The are also having same problem with LM318. How can I chose op-amps for those applications as well ?
Thank you.