Hi,
Simple, and maybe silly question: the data sheet for the THS4131 part shows a +/- 6V max input differential voltage (Table 7.1). I'm wondering if that's truly the case when operated with feedback and powered by +/- 15V rails? I would like to apply +/- 10V inputs. When I think of how an op-amp works with feedback, the 2 inputs are at virtual ground, so a true differential voltage present at the pins never occurs. So does this statement about +/-6V refer to a differential voltage present at the input pins, or does it refer to the differential voltage of an input signal that is present on the other side of input resistors?
Thank you.