Our customer is considering using the following in a new project of theirs.
1) THS9000 TEXAS INSTRUMENTS
Questions
1) Is the gain temperature characteristic of the data sheet, the typical value?
2) If there is data on the maximum value of the temperature change vs gain variation, the customer wants to see it. Data at 0°, 25°, & 50° is perferable.