Other Parts Discussed in Thread: OPA828, OPA4228, OPA189
Hi,
I'm after a faster precision op-amp than the OPAx197.
I'm after:
Ideally = offset < 1 mV ; 30 MHz ; Supply = +-15 V & +-12 at least - Quad package
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jean,
OPA828 with GBP of 50MHz and Vos of +/-150uV would be the fastest precision op amp but OPA189 (GBP of 14MHz) has highest precision of max Vos of +/-3uV. Hoever, neither one comes as a quad package. For higher bandwith quad version, we have only OPA4228 with GBP of 33MHz and max Vos of +/-200uV but it requires a minimum gain of 5 to be stable.