Hi Experts:
I'd like to know if the TL331IDBVRQ1 does support the AEC-Q100 standard or not , I didn't find any formation that this device support Q100.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts:
I'd like to know if the TL331IDBVRQ1 does support the AEC-Q100 standard or not , I didn't find any formation that this device support Q100.
Hi Jason,
Yes.
The TL331IDBVRQ1 is AEC-Q100 grade 3 (-40 to +85C) qualified.
The TL331QDBVRQ1 is AEC-Q100 grade 1 (-40 to +125C) qualified.
Devices in which the part number *ENDS* in "Q1" are AEC-Q100 qualified (but not necessarily grade 1 - some can be grade 3 or grade 0 - as in the TL331-Q1 case).