Other Parts Discussed in Thread: INA195,
Hi
customer is evaluating INA240, they want to get the curve as below, like INA195 curve.
could you provide INA240A2PWR, INA240A3PWR, INA240A4PWR curve?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Max,
Thanks for reaching out on the forum. I can check with my team when they return from their holiday vacation in about a week or so, but I do not think they have this data in a similarly processed form. The likely reason for this is that the INA240 is a bidirectional part that does not have region where the output vastly changes based on Vcm and the Vsense being under a certain threshold. However, the INA240 does have an offset voltage referred to the input and therefore Vout will not equal Ref + 0V for 0 A current. If you must have a graph to provide to your customer, I would recommend using the "INA240 Error Analysis" located on the right side of this page. There you can input your customer's operating conditions and export to excel the error curve data. From the that exported data you can then get the actual expected curve by subtracting the error percent from 100%.