Other Parts Discussed in Thread: REF2033
Hello
please give me recommendations about suply
i have :
~16-18bit ADC MCU
TI amc1301 for measure current shunt.
Shunt located in heavy EMI from random ultra HV sparks.
for power supply device i want use 1s Lipo
device shilded in metall box
i need maximum ADC perfomance for my situation
in this case i have some questions:
1. for accurate MCU ADC measurement i need external Vref.
in this case i can use dual Vref ic TI REF2033 (1.65V20mA + 3.3V20mA, 6 ppm/°C , Accuracy: ±0.05% ).
REF2033 out1 Vref 3.3 -> to MCU Vdda + amc1301 Vdd2
REF2033 out2 Vref 1.65 -> to MCU Vref
or amc1301 has internal precision voltage regulator , and i not need use any external Vref\Precision V source, and i can use low cost LDO without lost ADC perfomance?
or you can tell me a more optimal solution ?
2. isolated DCDC for isolated Vdd1 parts
3.3V to amc1301 Vdd1 from DCDC
i`m can direct connect isolated DCDC to amc1301 Vdd1 or for maximum perfomance also i need precision Vdd1 3.3 V source ?