Good morning,
i would like to use TLV316 opamp as comparator instead of finding for a comparator with push-pull output. My supply voltage is 5V, my input common mode voltage range is between 0V and 4V and the required output is about 5V or 0V depending on the comparison between the two inputs.
Are there some precautions or critical issue for this component if I will configure it in this way?
Thank you.