Hi,
The online INA381 Error Analysis does not allow you to enter a shuntresistor > 100mOhm
I have the following setup LNA381A4:
Sensed Current Range: 0mA till 30mA
Shunt: 220mOhm
Supply Voltage 3.3V
Common Mode Voltage:0V
Operating Temperature: 20±5°C
It it possible to provide me with a Error Analysis chart for this situation?
Or could you provide a tool which allows me to calculate situations without the limit in the online tool?
HJ