Other Parts Discussed in Thread: DAC60096, DAC43608, TLV9302, , TINA-TI
Hi Team,
My customer would like to proceed with TLV9302/4 with DAC60096 or DAC43608.
See below:
1. DAC60096 – The output signal of DAC60096 is (-10.5v) – (+10.5v) square wave so need TLV9302/4 to amplify the signal to 0-40v square wave follow the input, does is ok?
2. DAC43608 – The output signal of DAC43608 is 0-5v or 0-3.3v square wave so need TLV9302/4 to amplify the signal to 0-40v square wave follow the input, does is ok?
What the Vcc need for the TLV930x if the amplify signal need to be 0-40v? Can you do preliminary schematic for both options?
Does TI can prepare amplify board of 256 outputs (if use TLV9304 I believe need 64 ICs) that it will connect to DAC60096EVM or can prepare amplify board of 256 outputs (64 x TLV9304) with 32 ICs of DAC43608 because TI doesn’t have EVM for DAC43608?
Thanks,
Shlomi