Hi
I would like to understand the working principle of the circuit. The purpose is to use a current source(2.5mA) to check the 1 form C relay(1 Open, 1 Close, 6, 5, 4) status. Another relay is use to represent the status(right down corner). The input voltage is 24V at pin 7(left up corner). It seems R4 is used to control the current. Any unclear, please let me know.
Thanks in advance!