Hello
In the "SLOA059 –March 2001" it is shown the following text:
"Normal aging in semiconductors causes changes in the characteristics of devices. The input offset voltage long-term drift specifies how VIO is expected to change with time. Its units are µV/month."
Why is the information about "offset voltage long-term drift" not shown in the TLV2464 datasheet? Is it so low that it can be desconsidered or where can this information bee found?
I need it for the Vio calculation. See below.
Best Regards
Edson