Other Parts Discussed in Thread: TLV2772
Hello.
I have several questions regarding the datasheet/specifications for the TLV2772 opamp.
All question apply to a simple voltage follower configuration (IN- tied directly to OUT)
1) What would happen when VDD = 3.3V and IN+ = 6V (with a maximum current on IN+ of 4uA)? Does that potentially damamge the part, even though we're below the maximum VCC of 7V?
2) Similar question, but what if VDD was disabled (i.e. set to 0V) and we had IN+ of 2.5V (with a maximum current on IN+ of <2uA)? Would that also potentially cause damage?
3) Is the common mode input voltage limit actually VDD - 1.3V? The datasheet was a little confusing with the plus and minus signs. What are the consequences of exceeding that, say with VDD = 3.2 and a CM input of 2.5V?
Thanks,
John