Other Parts Discussed in Thread: TLV7041, TLV7031
I am looking at using the INA4181A1 (quad INA181A1) as a threshold current detector. I want to know when current exceeds a min level (~ 2 to 5ma). The current could be as high as 5A. Using a 10ohm sense resistor with a pair of schottky diode clamps. The supply is a bipolar PW encoded data stream from an H bridge driver. The diff input clamps ~.4v so the INA181 is driven to both rails. This is not a problem since I am not actually making measurements.
The spec sheet says output should return to normal ~20us after overdrive is removed. I ran a TINA Sim and found its taking ~25ms for the output to recover. I tried with and without 10k loads on the output.
Attached are screen shots of the circuit and plots. Am I missing something or is my sim flawed?