Other Parts Discussed in Thread: LM339
Hello,
I noticed the following description on LM2903-Q1's VICR - Common-mode input voltage range in the version H of the data sheet (SLCS141H).
It implies the inverting and the non-inverting inputs of the LM2903-Q1 are asymmetric. Is it correct?
If they were symmetric in terms of input structure, the description would be, "The upper end of the common-mode voltage range is VCC - 1.5 V for one input, and the other input can exceed the VCC level; the comparator provides a proper output state."
Best regards,
Shinichi Yokota