Hi,
I have a photodiode transconductance amplifier that I wanted to implement with a Microchip MCP601. Application is single supply +3 V. I wanted to use the quite practical configuration from figure 4.12, page 15 in the datasheet:
http://ww1.microchip.com/downloads/en/DeviceDoc/21314g.pdf
This is quite interesting as no additional (potentially noise-inducing) bias voltage is necessary. The trick is that IN- is driven slightly below GND by the photodiode, which in turn is being compensated by a positive voltage at the output. This works as V(CMR) is specified as Vss-0.3 ... Vdd-1.2 V. Of course the necessary range is only a few mV (or uV) below GND due to the high open loop gain (not sure how input offset voltage comes in play here).
As I have an LMV771 (774) elsewhere in the design (because I need the lower noise), I wonder if I can throw out the MCP601 and use the LMV771 instead (in order to reduce part count). Now V(CM) is specified as 0 - 1.8 V for the LMV771. The question is whether the LMV771 would also work with IN- slightly below GND as in figure 4.12 above.
Any ideas?