Other Parts Discussed in Thread: INA152, INA282, INA213
Hi,
I am trying to build a current sensor for a +/- 2mA sinusoidal current source injected into a 5k to 10k Ohm load. I am using the circuit shown in figure 29 of the datasheet for the INA197 (with a 33 Ohm shunt resistor) but getting some weird output from the INA197 which senses the negative-going phases of the sinusoid. The sensing of the positive-side by the other INA197 works great. The issue with the negative going output only happens for higher current values. Images below:
This is the output from the INA197 which senses the negative phases of the sinusoid.
Below are (yellow) the output of the INA152 and (cyan) the voltage waveform at the load.