Other Parts Discussed in Thread: LMP8602
The datasheet states: "The LMP860x and LMP860x-Q1 use level shift resistors at the inputs. Because of these resistors, the LMP860x and LMP860x-Q1 can easily withstand very large differential input voltages that may exist in fault conditions where some other less protected high-performance current sense amplifiers might sustain permanent damage."
What does "very large" mean?
I have an application where the current that needs to be accurately monitored is fairly small (mA) but can occasionally peak at 25 amps for a short duration (600 uS, using 10 mS as a design value). For the range of current monitoring I'm interested in, a current sense resistor on the order of 1 ohm would be appropriate. I have identified one that can handle the occasional (i.e. less than once per minute) power pulses without burning up. The part I'm concerned with is the LMP8602 amplifier. From a measurement perspective, I don't care that I'll rail the output at 5 amps, but I do care about survivability. Will the device be damaged or degraded by being subjected to a differential voltage of 24 or 30 volts?