Hi,
INA293 has a max BW of 1.3MHz and a slew rate of 2.5V/us.
If I calculate the maximum output swing at 1MHz, it is 0.397V, So If my Vout max is around 3V and output cannot swing to that voltage at a higher frequency. What is the use of having such higher bandwidth?
Also, In the datasheet, Section 7.3.1.1 explains Vsense vs BW but Figure 35 is BW vs Output voltage. It's a little confusing. (that voltage is Vdiff(sense )voltage or the output voltage of the Amplifier?
Regards
Vishal