Other Parts Discussed in Thread: ADS4222
Hi,
I am using THS4511 to drive ADS4222. My input signal swings from 0.9V to 1.8V. Since the input ranges near DC to 20 MHz, i decided to go for DC coupled operation with gain 0 dB. Also the source can't drive > 1 K ohm.
Considering this I decided to use 1K ohm for Rf and Rg for the amplifier feedback path. Since, the requirement of ADS4222 is that the input signal at input P and N should swing symmetrically around 0.95V common mode, I had to compress the range of input signal to the amplifier using a resistor divider configuration. Also Vcm output of the adc is used as vcm of amplifier.
Split supply of +3V(+Vs) and -2V (-Vs) is used for the operation.
I simulated the amplifer circuit in TINA and it gives me expected results. KIndly review my schematic and point out anything I may have missed regarding the proper operation of the circuit.Amp_Sch.pdf
Thanks and regards,
Vishak