Part Number: AM3352
Tool/software: Linux
Hi All,
First Version:
We have made a customised board with AM3352 processor, 1GB DDR3 and 512MB NAND flash. On our First version customised board we have made the setup working due to some hardware issue in the Ethernet section we have gone for the second version. We made SD Card booting done in first revision.
SYSBOOT : 0000001000110011 - NAND NANDI2C MMC0 UART0
Second Version:
We have made a customised board with AM3352 processor, 1GB DDR3 and 8GB eMMC flash. This is our second revision customised Board. Changes are done in Ethernet section and changed from NAND Flash to eMMC Flash.
SYSBOOT : 0000000000110111 - MMC0 SPI0 UART0 USB0
But when we are using the same setup the Booting Hangs in Starting Kernel.... .
What can be the issue ?
Any changes has to be done in U-boot or kernel?