Hi,
I have encounter a issue that the speaker have random pop noise occur sometimes during music playing.
I have record the I2S signal input to TAS2110 and confirm it is OK.
I captured the pop waveform on the speaker as below:
green is PVDD, yellow is speaker waveform.
amplifier configure as below:
I'm very confuse that if it trigger the OCP, the output should stop 1.5s and then recover, not just cause a pop noise. can you help to clarify what cause the pop noise. Thank you.