Tool/software:
I am trying to generate a tone on an 8-ohm speaker using ESP32 with I2S. Working conditions:
- SAIF: I²S
- 16-Bit Data, I2S_SLOT_BIT_WIDTH_32BIT
- RCLK = 48 kHz
- BCLK = 3.072 MHz
- MCLK = BCLK
But I was not able to get any audio and the fault register always returns bit 3 as active. The faultz pin is always high. However, I didn't find anything in the datasheet that could help. Does anyone have any idea what might be happening? Here is the I2S configuration.