This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Converter Apps,
Thanks for the sample code and advices in previous posts. The DAC output could now work and I could hear 48KHz recorded audio played out from the DAC, with exactly the same pitch as they were recorded.
|
|
proof |
|
MCLK |
18.4MHz |
oscilloscope |
|
Recording |
48 KHz |
|
|
CLKIN |
MCLK/2 |
Register 8: 42 |
✓ |
|
MCLK |
Register 8: 02 |
✕ Higher pitch |
This somehow confused me because TLV320AIC23B datasheet §3.3.2 describes tables in §3.3.2.1 as all based on CLKIN = MCLK, and I configured accordingly. However, the correct playback only happens when I choose CLKIN = MCLK /2.
Why could it be like this? Could you help me to figure out the reason?
Zheng
Hi Zheng,
I agree with your analysis. This doesn't look right. Perhaps there is an issue with the other clocks or some programming in the micro? You could try setting the AIC23B as the master and looking at LRCK with a scope to see what sample rate the AIC23B thinks it is running at in both conditions.
Converter Apps,
Thanks for confirmation. I will test on this some time later.
Zheng
Hi Converter Apps,
I encounter the same problem with Zheng, and now I set AIC23B as the master device and choice USB mode, but my headphone has only Left channel out, Right channel has noting out? I don't know why?
Fang