This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5727: Could not pas HD DTS test

Part Number: TAS5727
Other Parts Discussed in Thread: TAS5538, TAS5352,

Our customer has done the HD DTS certification test, but has failed. While another one TAS5538+TAS5352 has passed.

In the test, the signal source will output 3 kind of signals in different frequency (30Hz, 1KHz and 12KHz), the load is 8Ohm and power is 1W. The requirement is the harmonic wave at other frequency must not exceed its range. But in the test results, harmonic wave at 10kHz and 14kHz is beyond the requirement. (requirement is not exceeding -70dB, but actually is exceeding -60dB).  While for TAS5352, both under -80dB.

Please see attachment.

In addition, power supply is 20V. And it has passed EMC test.

Look forward for your replying.

Thank you.

8 ohm 3 tone for 5727.pdf

8 ohm 3 tone for 5352.pdf